Trico Corporation logo

Cleaner Oil.
Better Equipment Performance.

Portable filtration provides a practical way to remove contamination while oil remains in service.

Trico filtration systems help remove particles, moisture, and other contaminants from new and in-service lubricants. Improve fluid cleanliness, support equipment reliability, and help extend lubricant service life.

For new and in-service lubricants
Portable and dedicated filtration options

Clean the Oil,
Not Just the Machine

Gearboxes, hydraulic reservoirs, circulating oil systems, and other lubricated assets are continuously exposed to particles, moisture, and other contaminants through normal operation, reservoir breathing, maintenance activities, seals, and the surrounding environment.

Changing the oil removes the contaminated lubricant, but it may also mean disposing of oil that still has useful service life. Portable filtration gives maintenance teams another option by circulating existing oil through appropriately selected filtration media and returning cleaner oil to the reservoir.

Contamination alone does not necessarily mean the lubricant has reached the end of its useful life.

A single portable system can potentially move throughout the plant and support multiple compatible applications, helping make filtration part of planned maintenance instead of reserving it only for contamination emergencies.

Shop Portable Filter Carts
Trico portable cart and handheld filtration systems
Maintenance technician sampling oil from a handheld filtration system
Trico high-viscosity filter cart connected to industrial equipment

Why Add Filtration to Your Lubrication Program?

Address contamination before it becomes a larger maintenance problem.

Remove Contaminants

Remove particulate matter, water, and other contaminants from lubricants.

Support Fluid Service Life

Keeping lubricants clean can reduce the need for frequent fluid replacements and maintenance.

Help Reduce Waste

Prolonging fluid life can decrease the environmental impact associated with lubricant disposal.

Move Between Assets

Use one portable system across multiple compatible applications as maintenance needs change.

Choose the Filtration Format That Fits the Work

Trico offers portable and dedicated options for different maintenance requirements, lubricant viscosities, storage needs, and transfer activities.

Trico portable cart-style filtration system
 

Portable Filter Carts

Move filtration between compatible assets and incorporate oil cleanup into planned maintenance.

Shop Filter Carts
Trico portable handheld filtration system
 

Handheld Systems

Bring compact and convenient filtration to compatible lubrication applications.

Shop Handheld Systems
Trico panel-mounted filtration system
 

Panel-Mounted Systems

Provide dedicated filtration directly at compatible equipment.

Shop Mounted Systems
Trico drum pump filtration system
 

Drum Pump Systems

Filter lubricant during storage and transfer before it reaches the equipment.

Shop Drum Pump Systems

From Contaminated Oil to Cleaner Oil

Clean the lubricant while it remains part of the asset's lubrication program.

1

Before Filtration

Contaminated oil circulates through the system. Particles and moisture can contribute to wear and reduce equipment reliability.

2

Filter While in Service

Oil circulates through the filtration system to remove contaminants, then returns to
the reservoir.

3

After Filtration

  • • Improved cleanliness
  • • Extended oil service life
  • • Improved equipment reliability
Trico filtration case study showing oil cleanliness results before and after filtration

Documented Filtration Results

In one Trico case study, purchased gear oil was filtered with a high-viscosity handheld system. The results below apply to that documented sample and filtration sequence.

1

Starting Sample

ISO cleanliness code 20/19/15 with a wear particle concentration rating of 7.8, classified as marginal.

2

After 10-Micron Filtration

After two hours of filtration, the oil measured ISO 18/17/14 with a wear particle concentration rating of 7.3, classified as normal.

3

After 3-Micron Filtration

After an additional two hours of filtration, the oil measured ISO 17/16/14 with a wear particle concentration rating of 3.3, classified as normal.

Trico reported only trace quantities of debris in the final sample, with no signs of steel or nonferrous debris observed.

View the High-Viscosity System

Portable Filtration FAQs

Quick answers for maintenance and reliability teams evaluating oil filtration.

No. Contamination alone does not necessarily mean the lubricant has reached the end of its useful life. When oil analysis indicates the lubricant remains suitable for continued use, filtration may help restore cleanliness without automatically replacing the oil.
Portable filtration offers flexibility. A single system can potentially move throughout the plant and support multiple compatible applications, which can help facilities address numerous lubricated assets without permanently installed offline filtration on every machine.
Consider gearboxes with large lubricant volumes, critical production equipment, hydraulic reservoirs and equipment operating in dusty, humid or challenging environments. Start with a few assets where contamination could have a meaningful effect on reliability.
Consider filtration when oil analysis indicates elevated particle contamination, after maintenance work exposes a reservoir to the environment, or when in-service oil remains suitable but needs improved cleanliness. It can be part of planned maintenance as well as a response to contamination.
Oil analysis and particle counting can establish the oil's current condition, help define the required level of cleanliness and verify whether the filtration work accomplished its objective.

See Trico Filtration Solutions

Watch these Trico videos to learn more about lubricant filtration systems and their use.

Portable Filtration

Explore Trico Portable Filtration

See how portable filtration can support cleaner oil in industrial
lubrication programs.

Filtration Systems

Learn More About Trico Filtration

Review another supplied Trico resource covering lubricant filtration.

DISCLAIMER: The above content is provided by the supplier. Applied® does not guarantee the accuracy or timeliness of the content.
The above content is provided “AS IS”, AND ANY AND ALL EXPRESS AND IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS ARE HEREBY EXCLUDED.
All warranties, if any, are solely from the supplier.

Find Your Local Applied® Service Center

Locate your nearest service center to get hands‑on support, product guidance, and industrial solutions.